Other Parts Discussed in Thread: PCM3070, TPA3100D2, PCM3070RHBEVM-K
I've got a problem with the PCM3070. I opened in the Pure Path Studio the example /Parametric EQ
If I change the Gain Parameter of the Equalizer,there is no change.
The second problem is, when i Download the Code into the chip, I must Route the Audio Outputs in the PCM3070-K Control Software again.
Did i do anything wrong?
At the Moment i have the PCM3070RHBEVM-K Eval KIT and connect the headphone output from my smartphone to the IN1L und IN1R. Then I want to go through the EQ and the LOL and LOR into the Amplifier (TPA3100D2)
Hope anyone can help me.