Hi,
can anybody tell me the imput impedanz of the LME49990, want to use it as elektrometer/non inverting amp. Thanks a lot.
With best regards
Gerhard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gerhard,
I am looking into this for you and will provide information as soon as I have it.
Thanks and Best Regards,
JD
Hi Gerhard,
The common-mode impedance is in the hundreds of Mohms while the differential mode is around 10 Mohms.
Best Regards,
JD
Hi John,
thanks.
One more question. I need a differential circuit, so I take two LMP49990, because noise is an issue. I found out by simulation, that I need a relatively small resistor from + input to fround. Why? I use the amplifiers as non inverting amps with gain 100. The outputs go to an THS4131 for further processing, filtering and ends up in a sigma delta ADC (24 Bit) which also offers true differential signal path.
This resistor bring down my input impedanz which should be about 1M ....
Now I tried OPA827, which is recommended for high impedanz sources, because its current noise is low.
Did you have another idea to do the job?
With best regards
Gerhard