Extended question
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Extended question
Fritz,
I'm not sure I understand what you're trying to do. Are you trying to hack into this controller board to add extra toslink inputs?
-d2
Hi Don,
Indeed, I'm trying to extend the functionality of the board. But it also seems to be possible to create a "shell" before I enter the board. My Panasonic DVD-player, AppleTV, Apple media server and Cyrrus high-end CD / SACD player all have a TOSLINK digital output. I think it's better to use these, then their analog RCA output and converting Analog to Digital on the TI board. I think only my vinyl record player and the radio tuner shall use the Analog/Digital converter of the TI Board. Of course it is possible to use an external TOSLINK splitter, but these are rather primitive. And after all, I'm trying to integrate the maintenance of all my devices into one (1) control-unit (maybe it's possible to interconnect and integrate the three corresponding HDMI-resources too).
Thanks for your fast respons,
Yours sincerely, Fritz T.
p.s. I've ordered the TAS5631DKD2EVM - TAS5631DKD2 Evaluation Module to find out the possibilities.
Hi, Fritz,
Sounds like a fun project!
It might be easier to make a new PCB rather than trying to hack up the INPUT USB Board.
Good luck with it.
-d2
Hi Don,
Seeing the board I received yesterday, I think you are certainly right ! So I think I'll better work on a "shell". It will take some time to understand the working of the board. It's a nice job for the christmas vacations. Meanwhile, if you have some information / threads how to address three TOSlink inputs to the single input of the board, I'll be glad to hear that.
Thanks so far !
Yours sincerely
Fritz T.