Other Parts Discussed in Thread: TPA3123D2
Hello! I'm mounting a prototype according to the evaluation module for TPA3123D2 and there are some issues. Once the prototype was finished it begun to oscilate with a small pulse about 3.8Hz, without sound. To remove this, I simply disconnect the 1 uF capacitor (C6 to pin 11 VCLAMP) and it started to work properly. Can this pin still unconnected or what kind of capacitor do I need?
That's the minor problem, the mayor problem is when I try to set any of the gain inputs to VCC the amplifier starts to oscilate, blocking the sound. Only works well when that inputs are tied to GND. In addition to this, the normal consumption is about 50mA
but when the jumpers are open (so +12VCC pull up) the consumption rises to 500mA causing undesirable heating of the chip.
The output configuration is single ended.
Any suggestions?
Thanks in advance.
Carlos Vargas