Dear TI,
My Company, ELK Industries, LLC (www.elkindustries.com) Purchased one of the TAS5615DKD2EVM - Power Amplifier Evaluation Circuits.
Now, it has ceased to Function. The (ONLY) Clue, as to it's "STATUS", is that the FAN (+12 VDC) which is unused Measures only + 5.5 Volts DC.
How can We arrange to have the EVM (Module) Serviced? It Cost US >$300 or so, when we Bought it ! Now, even though Power to it, Inputs, and Speaker Connections have been Checked, and Doublechecked, it does not Produce any Output. The Circuit was Used for several Months, Successfully, with a +50 VDC Heavy Duty Regulated Power Supply. The POWER SUPPLY is FINE, Yet the Amplifier Module is "DEAD".
PLEASE ADVISE.
Thank You kindly,
******************************** LASEROB !!
Mr. Robin Elkins, CEO
Elk Industries, LLC
221 W. Hibiscus Blvd.
#106
Melbourne, Florida 32901
United States of America
321 259-8114 or 321 259-8101
FAX: 321 723-2739
Email: LASEROB@aol.com
www.elkindustries.com