This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3112D1 design information - ???



Does anyone understand how the PLIMIT voltage is used and the power output calculated together with the o/p voltage amplitude as per table 2 in the data sheet SLOS654C. I must be having an off day because I cannot find any useable data regarding this subject. Any derivation of the figures in the table would be helpful, I shall be using a 12V system target output power is 20W into 4 ohms.

So, I see one confusing entry in table 2 when comparing it to Figure 9 in datasheet, the 4th line of table 2, Vplimit should read 3.5V (approx) which is close to what I would guess at.