We are going to use an AIC3254 Codec in our system and I am currently working on the software for the codec in PurePath. My problem is this: we will be using non-standard sample rates through using the internal PLL. PurePath, though, seems to only support the standard sample rates of 8, 11, 16, 22, 24, 32, 44.1, 48, 88.2, 96, 176.4, and 192 kHz. Is this a problem? Should I just tell it the nearest sample rate to the true sample rate?