Hi
Currently I use CC8531+AIC3204, I want to Configure it as two Mic input to one output, how can I do in PurePath Wireless Configurator?
Thanks
Gary Siu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Currently I use CC8531+AIC3204, I want to Configure it as two Mic input to one output, how can I do in PurePath Wireless Configurator?
Thanks
Gary Siu
Hi Gary,
This is available as choices in the PurePath Wireless configurator.
Start off with the CC85XXDK-Headset, preloaded demo as your project.
This will work using the CC85XXDK-Headset development kit, but similar approach can be done for a custom design,
For the master:
1. Select 'Stereo Output base statio' from upstream audio as configuration type
2. In audio streaming panel, set logical channel to mircophone 0 and 1 with AD1 as Audio IO
3. In Radio panel, set maximum slave count to 2
For the slave:
1. Select 'mono microphone' from upstream audio as configuration type
2. In audio streaming panel, select Automatic for dynamic selection
You should now be able to pair two slaves to the master and send a mono channel from each.
Let me know if you have any questions on this.
Best regards,
Kjetil