This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pcm1774 problem

Other Parts Discussed in Thread: PCM1774

Hello,

I'am trying to connect a pcm1774 to a stellaris mcu over spi. The mode pin is connected directly to ground. CS, MOSI, SCK are connected to the MCU. All power supplies (VIO,VDD,VCC,VPA) are connected to +3,3V. The other pins pins 9 (SCKI), 10 (BCK), 11 (LRCK) are not connected until know. I'm trying to power up the VCOM over the register setting: 0x4A01, but I still can not measure voltage on pin. So I think the dac don't unterstand the message, but I don't know where I'm wrong. I'm using SPI Mode 0(SPO=0 and SPH=0).

Can anyone help?

Attached a measurement of the SPI Interface: