hi,
i have made an amplifier of 60W+60W using LM4780 with refference from the application ciruit from the data sheet.
i have tested the board with 34/0/-34 volts supply at 4ohms load, sound quality is good but less power comared to 20W amplifier TDA2030.
again i have tested the board with 12/0/-12 volts supply at 4ohms load, the sound quality is good but output power is same.
what is the problem with design ?
gain is 21, all connections are good.
can i any one tell me, did you have the same problem before and what is the solution ?