We are using a TAS3108 in an application which would benefit from using the DRC as a distortion limiter. I've read the "DRC help" section within TI's PurePath Studio, as well as searched the forums here - including the SLOA148 DRC application note for the TAS57XX. But, I'm still a bit uncertain of how the available parameters impacts the audio processing.
1) Measurement of Peak or RMS. I would assume a distortion limiter should use "Peak" as opposed to RMS? It seems this variable, in conjuction with t_energy, would create a time-averaged/filtered version of the input signal - is that right?
2) Compression Ratio. I'm assuming you would want to set this to the amount of max compression needed for a prescribed amount of distortion with a maximum input?
3) Threshold. Is this used relative to the Peak/RMS measurement version of the signal? What is 0dB related to, the max output of the DSP (0 dBFS)? Does it make sense that one could adjust this until the maximum amount of desired distortion was determined using sine waves?
4) t_energy. Is this the size of the time window for averaging the input signal? So, for a limiter application, one would want this shorter (100-200 ms) - rather than longer (1000-2000 ms), right?
5) t_decay. While I understand this would dictact the rate of attack, I am unsure how to determine the attack "slope" (dB/ms) if you will. Can the slope be calculate based on this variable and the Compression rato? Thus, 10 dB of compression and 10 ms attack time gives 1 dB/ms rate of limiting?
6) t-release. Same as #5, but with respect to limiter release
In general, it seems to create a distortion limiter, I would want to input a signal level where output distortion begins. I would then lower the DRC threshold to determine where to initiate the limiter at the desired amount of distortion. I would then increase compression ratio until that distortion is reached through maximum input. Then attack/release controls the "dynamic agressiveness" of the limiter.
Any other insight or suggestions would be appreciated.