i wanna use USBMODEVM at 96 kHz and maybe at 192 kHz ... is this possible ?
and where to find the firmeware files for this frequencies (USBMODEVM0202_96KHZ.BIN and USBMODEVM0202_192KHZ.BIN ?? )
thx,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i wanna use USBMODEVM at 96 kHz and maybe at 192 kHz ... is this possible ?
and where to find the firmeware files for this frequencies (USBMODEVM0202_96KHZ.BIN and USBMODEVM0202_192KHZ.BIN ?? )
thx,
Hello Pascal,
The USB full-speed interface does not allow stereo, full-duplex 96 kHz (or higher), 16-bit isochronous audio data due to bandwidth limitations. That is the reason why there is no 96 kHz firmware file for the USB-MODEVM.
Regards,
J-
Ok, thx for replying.
so, i'm trying tu use EVM by this way:
-audio generator linked on IN1L
-audio analyzer linked on headphone output Left
-Purepath config: (a bypass in fact)
samplerate : 176.4Khz
framework : AIC3254App2x1x
input : MonoDec1xIn
interprocessor : MonoDSP_A_DSP_D2x1x
output : MonoInt2xOut
this works nice, except that this bypass is a low pass !
| Freq in kHz | dB output |
| 2 | -5.8 |
| 10 | -5.8 |
| 20 | -5.8 |
| 24 | -6 |
| 28 | -7 |
| 32 | -9.3 |
| 36 | -13 |
| 40 | -20 |
| 44 | -31 |
| 48 | -52 |
| 52 | -63 |
| 56 | -67 |
| 60 | -80 |
what is wrong ????
humm, i understand my mistake: it's not the good component for my application ...
it's an "audio only" chip