Other Parts Discussed in Thread: USB2ANY
We are designing an audio product using Stellaris, Bluetooth, and the LM48901.
While using the eval boards, USB2ANY, and the control GUI are instructive on how the LM48901 works, our final design will not have the connection to the GUI over USB2ANY; LM48901 control and register writes will be over I2C from the Stellaris. The plan is to store the spatial coefficients as an array in the Stellaris flash, and load them into the LM48901 with I2C. However, I have no idea of the format of the Tap and Prefilter Tap data, or how it is stored in the .dat files provided by the online tool. The data sheet's 6 rows in a table are not sufficient for describing the coefficient memory.
What I need at this point is information that will allow me to:
1. take a coefficient file and create an array in C-code format for loading into the Stellaris as part of our control application
2. use the I2C to load the array of data into the LM48901's coefficient memory using the I2C connection.
Can anyone point me to said information via links, attached pdf's, etc.?
Thanks