Other Parts Discussed in Thread: PCM1794A
I have a question regarding PCM1974A datasheet. Is the internal digital filter running at 8x oversampling ratio even at the maximum input sampling rate fs of 200KHz? The oversampled signal rate between the digital filter and the multi-level sigma-delta modulator would then be 1.6MHz. High performance audio DACs from other companies seem to run at lower oversampling ratios at high input sampling rates, so that the output rate of the oversampling filter is kept relatively constant. A somewhat related question is whether the maximum fs of 200KHz also applies to the external digital filter mode, where the frequency of WDCK can be either 4fs(800KHz) or 8fs (1.6MHz). If not, what is the upper limit for WDCK frequency in external digital filter mode? Thank you.