I have a house next to a highway and I was going to setup an active noise cancellation setup outside to cancel the highway noise so that the yard would be quiet. I was wondering if somebody could give me an idea of the zones I need to create. Should I use more than one board, or should I attach multiple speakers and microphones to one board. Should the speakers just face the highway or do I need to have speakers facing multiple directions. I would appreciate any feedback greatly.
Thanks
Alex