I've been looking at the PCM2902 ( http://focus.ti.com/lit/ds/symlink/pcm2902.pdf ) ADC and I'm wondering what the input impedence of the chip is in the off state? I'm concerned that if powered down, the chip may load down whatever circuit is connected to the input.
The input impedence is listed as 30kOhm, but since there isn't any information on how the ADC is designed, do any TI designers/engineers know whether the input impedence will rise or fall?