Other Parts Discussed in Thread: PCM9211, PCM9211EVM-U
Hello,
I hope this e-mail finds you well.
My client intends to use PCM9211 using auto source selector for their audio product
- PLL srource/ RXIN2 SPDIF( Optical) 48KHz 256fs
- ADC fs= 96KHz 128fs slave mode
This operation looks fine in the PCM9211 EVM-U ( also their product), however, .. when client plugged in/out the Optical source (cable)
so frequently ( 1 times/sec x 100~200 times), output from Main Output Port was losed ( stuck to GND)...
And also, PCM9211EVM-U Lock LED does NOT distinguish ( i.e. indicates Locked ).
Problem is there are no way to detect the error from PCM9211 to MCU.
This situation can be solved by
* Hardware reset ( 0x40h; system reset can't solve)
Or
* 0x26h changed from 41h to 01h ( AERROR Not slected ),, and
* 0x25h changed from 23h ( EFSCHG,=1 EPARITY=1) to 01h
Would you please let me know the cause, and register setting for AUTO_detection?
Clients are in hurry ( Before Mass Production ) and hope to your reply within 3 days
Best Regards
PS
Client's setting is below in the PCM9211EVM-U
w 80 23 05
# 05h
w 80 24 10
w 80 25 23
w 80 26 41
w 80 28 05
w 80 2A 1F
w 80 30 02
w 80 31 15
w 80 32 22
w 80 33 11
w 80 34 02
w 80 35 02
w 80 6D F0
w 80 6E 00
w 80 6F 80
w 80 78 3E
w 80 6B 00
If you had any queston, please let me know.
Sorry to bother you, but with my best regards