I am trying to run the examplecode ADC_I2C_VOL_DAC in PurePath.
The code seems to compile and download as expected, but I can not get any audio signal out of it from PurePath on any output.
I have connected a input signal to IN1 and I am listening on both LINE-OUT and Headphone output on the EWM board.
(When I use the software tool 'AIC3254 Control Software' all analog routing from the input to the output is working as expected including analog bypass around the ADC-DAC with help of the MAL/MAR routing)
- How do I configure the analog input/output paths in PurePath ?
- Which frequency of the masterclock does PurePath expect ? (And how do you use PurePath code in a inbedded soultion with another frequency) ?
PS. I have read the User Guide and so on for PurePath, but some of that information seems to be for an older CODEC. DS.