I am using CC85XXDK-HEADSET.
When I brought two pieces of boards close, there was a case where connection was impossible.
I experimented.
It turned out that the phenomenon which I cannot connect from this experiment changes also with direction.
The result of an experiment is expressed to lostconnection.pdf.
Is this cause CC8531? I would like to know.
If it is right, is there any measure method?
I appreciate your kind cooperation.
hirokuni.oota