Other Parts Discussed in Thread: TPA2038D1, TPA2037D1, TPA2039D1
Hi community
I'm designing an audio amp for cellular phone application which will need two amps - it's a security device which has a very powerful rear speaker in addition to the standard speaker you'd put on your ear. Due to the high current consumption, I can't use an audio switch, so I need two separate amps connected to the same audio source (see schematic below). These will be switched with the respective amp enable signal.
Now, I'm not sure if I can just connect the two inputs together in this way. Would there be any interference from the other amp (which is in shutdown mode) when using one amp at a time in this configuration?
Inputs are connected together after the input Gain conrol / HPF to save components. I'd like to keep it that way, but if it helps I could interconnect the amps before the gain / hpf circuit and add one circuit for each amp.
The Audio source signal is the output from an audio voice codec IC (MAX9860).
Any help is much appreciated!
regards
Jonathan Bischof