Hi!
I use TPA3123D2 and i've made a couple of PCB with it. It works well but i noticed it's too warm even when there's no sound at all. Still it stays warm even in mute mode. I can see supply current about 60mA but datasheet says 23mA. The conditions are follows:
Supply voltage 24V
Single ended configuration
SD pin stays at +3.3V level
Mute pin stays at +3.3V level
All the PCB is made with TPA3123D2 evaluation board recommendation, layout and BOM.
Output filter is made with good SRR1208 22uH inductors and ceramics 1206 X7R 0.68uF.
What did I do wrong?