Other Parts Discussed in Thread: CC8520, CC2591
Hi,
Does the CC8520 use the Spread Spectrum technics?
Because as I saw on Configurator, have 18 channel for use.
Thanks,
RF_pts
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The 8520 uses adaptive frequency hopping. You can find a nice description in section 2.4.3 of the users guide
http://www.ti.com/litv/pdf/swru250l
Regards,
BK
Hi RF_pts,
Yes you can. The Wireless Commander allow you to test all EHIF commands and RFT_NWKSIM is designed for your purpose. See the CC85xx User Guide appendix B for EHIF reference and the commander built in help system for usage. Using the built in script editor or the command and monitoring panel is probably the fastest way.
Regards,
Kjetil
Hi Kjetil,
Thank you for your clarification. It´s very useful for me.
Yes, I tested these procedure, works fine. Since I have only one CC debugger in my hands now, I couldn't check the tx signal, but I am monitoring the CC2591 PAEN pin using a scope.
Maybe tomorrow I'll have the 2nd CC debugger, so I hope test the RX and TX.
Could you clarify another issue? As shown on PPW Configurator, all 18 channels has a start freq and end freq. But these values don't match with the PPW Commander.
Example: Channel 9 on PPW Commander use 2.442 GHz, but in PPW Configurator the range for change 9 is from 2.436 up to 2.440GHz. This happens also on channel 18 - I'm referring to prod_test_simplerf_tx configuration loaded in Product test screen of the PPWC Commander.
Thank you.
Regards,
RF_pts
Hi RF_pts,
The PurePath Configurator have the correct frequencies and there seems to be an bug in the commander scripts. Some of the EHIF commands related to TX/Rx has finer grain adjustment than just channels (specifies direct frequencies instead) and assume that is where the errors where introduced.
Quick fix is just to edit these yourselves. They are .xml formatted files that can be found here:
C:\Program Files (x86)\Texas Instruments\PurePath Wireless Commander\config
Just to make it clear:
Channel 1 2406 MHz
Channel 2 2410 MHz
Channel 3 2414 MHz
Channel 4 2418 MHz
Channel 5 2422 MHz
Channel 6 2426 MHz
Channel 7 2430 MHz
Channel 8 2434MHz
Channel 9 2438 MHz
Channel 10 2442 MHz
Channel 11 2446 MHz
Channel 12 2450 MHz
Channel 13 2454 MHz
Channel 14 2458 MHz
Channel 15 2462 MHz
Channel 16 2466 MHz
Channel 17 2470 MHz
Channel 18 2474 MHz
Regards,
Kjetil