This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC36 - Access to miniDSP processed data and interface to Raspberry Pi

Hi All,

Could someone help with two questions?

1) The TLV320AIC36 can sample audio at 32 bits / 48 KHz then pass internally to its miniDSP then pass the output of the miniDSP to a host processor such as the Raspberry Pi (and reverse for audio output)? Or is the data path to a host processor restricted to audio data only (not the output / input of the miniDSP)? 

2) Interfacing to the Raspberry Pi is reasonably accomplished via the I2S implementation on it? I understand you are not the makers of the Pi. Perhaps someone here has experience with it.

My goal: real time studio quality audio input and output with custom code running on an off the shelf inexpensive Linux machine in between.

  • Hi, Perry,

    1) Figure 1.1 shows the output of the ADC and the input of the DAC can be routed out thru i2s, so, yes, this is possible.

    2) This should be ok as long as you understand i2s is meant for short runs on a PCB. Running it across long wires and headers and such may impact audio quality.

    -d2