Purchased TI Codec EVM kit TLV320AIC36EVM-K
I'm unable to install the drivers for the board and the codec. I followed the user guide documentation step by step (section 3). I'm using all the default settings powering it over USB. When connected I see a few leds light up (D3, D4, D5, D7, D8).
I also followed the TLV320AIC3xEVM-PDK Series Troubleshooting Guide. In section 3.2 it says that i should find two files:
a. C:\WINDOWS\system32\drivers\NiViUsbK.sys
b. C:\WINDOWS\inf\USB-MODEVM_WDM.inf
I can only find b. That might indicate an issue with the installer. I tried to uninstall/reinstall with no luck.
To reproduce:
1. Installed the software provided at http://www.ti.com/tool/tlv320aic36evm-k
TLV320AIC36EVM-K - Graphical User Interface (GUI) Software (v1.2.0) (Rev. A)
2. Connected codec to the board.
3. Connected USB cable
4. Windows presents a dialog saying it detected new hardware. I select not to use auto search. The wizard says it's Unknown and won't install the driver.
Please help,