I am using a PCM1792 in a non-audio application, a product which will generate signals up to 80kHz. I am seeing higher noise than I expect. When 0V is commanded from the DAC it generates near zero volts but there is noise on the DAC's output buffer (before the anti-imaging filter). The noise is roughly 80mV p-p in the area of 800kHz to 1.8MHz.
The question is, is this to be expected?
Is it a result of the digital filter?
Is this the source of limit cycles or idle tones?
Or am I doing something wrong?