This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM49352 - Using the LM49352-I2C-Interface-Software

Hi,

I am preparing for getting my prototype of LM49352 to run. The software for setting the registers (snac24.zip) is ready to use, the only thing that is missing is the right interface between the PC and the board (some USB-I2C-Interface) but I could not find any hint on what (USB)interface has to be used or which one is know to be working.

Unfortunately, there is nothing available within the software (V1.0).

I would be glad to get any support on this.

Thanx in advance!

Bye

Claus

  • Hi, Claus,

    Unfortunately, that s/w requires the use of an interface board which is now obsolete (that's why there is no EVM listed in the Product Folder). I will have it removed to eliminate future confusion.

    My suggest is to get an I2C to USB writer, and write the registers directly. Sorry that we don't have an easier way for you to do this...

    -d2