This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bug in CC85xx



I have a few of "Purepath Wireless Audio EB 1.2" boards. I tested the system in a simple configuration with one master as an audio source and two slave as wireless speakers. The distance between the master and slave was like one meter. On these boards there is a green LED indicating the connection status. When the LED is on constantly, it means that they are connected and the slave is consuming an audio channel. I could hear the audio signal through a headphone.

The problem I observed was that, during my testing for like 40 hours, I could not hear the audio signal at the slave side for like 3 times and as soon as I reset the slave every thing was fine again. 

I would like to know if this is a known bug or does anyone have exprienced a similar situation.

PP configurator version: 1.4.1

CC85xx Device revision: 2.0