This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5508C EQ GUI

Other Parts Discussed in Thread: TAS5508C, TAS5558, TAS5548

Dear Sir,

Is there EQ GUI tool can help TAS5508C EQ fine tune ?

ALE 5.2 generated EQ file format is not same as TAS5508C EVM tool.


Many thanks !

  • Hi, Terry,

    For mature devices, we are not developing new tools.

    The tools are much better for the newer devices, TAS5548 and TAS5558. I suggest you look into those devices.

    -d2

  • Hello Terry:

    I'm not sure what you mean by the format is not the same.

    ALE 5.2 gives you 20 biquad coefficients but it arranges the biquads in 5 rows with 4 bytes of coefficients per row.

    The TAS5508C GUI has only one row with a register number preceeded by "X" and followed by 20 bytes.

    If you want to use ALE 5.2 and convert to TAS5508C format, this is the following format:

    XYY ZZ ZZ ... ZZ

    X - is required to denote a new register

    YY - register number

    ZZ - byte of data (for the EQ biquad, there are 20 bytes; ALE 5.2 first 4 bytes on the top line go to the first 4 bytes right after the register number in the GUI format, and so on).

    Best regards,

    Tuan

  • Hi, Terry,

    This might help you:

    Use ALE5.2 and save it as cfg file in the below format and use the tool to download to the device.

     

    XYY ZZ ZZ  … ZZ

     

    X – must have this character capitalized

    YY – the register number

    ZZ – the 20 bytes data for the coefficients

     

    -d2

  • Hi Don Dapkus,

    Would you suggest how to set DRC for TAS5508 GUI ?

    I use ALE to generate a DRC file for TAS5508 GUI and load it, can't see any effect ?

    Many thanks a lot !