Other Parts Discussed in Thread: CC2590
Hi ,
As I known in the application note AN089,for the CC85XX the LOS range is 35+m and 130+m when adding cc2590. I have a question :the LOS range of 130+m ,did the MASTER and SLAVE both contain the cc2590 ? If I used the MASTER which contains cc2590 and SLAVE without cc2590, will the LOS range be shorten? Dose the SLAVE RF output power effect the distance of stable conection,for the "ANSWER" from the SLAVE cann't reach the MASTER? I want to reduce the cost by remove the cc2590 from SLAVE,but I worry about the action may short the link distance. Hope for reply,thanks.
Best regards
Jack.