This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1018 case temperature information

Dear support team,

May I have your support to check how we can specify the recommended operating temperature on IC case? 

Our datasheet only list the junction thermal impedance and specify the free-air temperature range. Could you kindly help to check this for us? Thanks!!

Supply voltage:                                                         –0.3 V to 5.5 V
VIN Input voltage:                                                     –0.3 V to 0.3 V
θJA Thermal impedance, junction to free air:    230.47°C/W
TA Operating free-air temperature range:           –40°C to 85°C
Tstg Storage temperature range:                         –65°C to 150°C

Best Regards,

Dan Lu