This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue Connecting PCM2900C Using WindowsXP Embedded

Other Parts Discussed in Thread: PCM2900C

Hello,

I have a new design using the PCM2900C USB Audio CODEC and have tested the circuit using Windows Vista with success.  The target OS, however, is WinXP Embedded and I am having an issue getting the device to properly work on the XPe platform.  Using Device Manager, I have the "USB Audio CODEC" showing up (with a ?) in the "Other Devices" section, so, it is there and being recognized by the OS.  However, I cannot get any driver to work with the device and end-up with Windows -28 error (no driver found).  I've tried to install the software on the PCM2900C page (Filter Driver Update), but with no luck.  Is there another driver available or can someone offer advice as to the precise drivers required and where I might locate them?

Thanks