Hello Kristoffer, Kjeti,
This is regarding the old post that i have published in TI, http://e2e.ti.com/support/low_power_rf/f/382/p/105870/848681.aspx#848681
I would to reopen the topic and need your extensive support.
With your code provided, we have established the project and facing few bugs that need to be cleared.
1. Network status LED is configured along with the Volume up button in the code ( which is not apt )
in our board Network status LED is configured to GPIO12 but the port is not enabled to edit with the Purepath configurator.
2. The Power toggle button is not working, CSN is configured for power on function in Hardware as well as the SW (Hold functionality is assigned) but whenever the button is on hold, the clock seems to turn on, where as when the button is released the clock dies.
It seems to be there is some mis - porting which creates the bug.
could you support me for the software to ensure the 4 microphone configuration.
thanks,
Best regards,
Winnefred K