I have been working with a PP wireless CC8520 + CC2590 chip-set design for some time now with great reliability. I'm confident in the design and was able to solve problems during development with TI's help.
We have tested with a single master and single slave, and both RF PCBs are enclosed in MDF cabinets.
The RF antenna is internal to the PCB based on the suggested design from TI.
Reliable audio play with no dropouts with clear line of sight between transmitter and receiver has been measured to 65 ft (19.8 meters).
The transmitter and receiver will connect and play up to 111 ft(33 meters) but if a person walks between the units it will drop out.
Reliable audio play with no dropouts between a single house wall between the transmitter and receiver has been measured to 36 ft(11 meters).
Now that we have gone into production, we are seeing a degradation in this performance, and are now getting audio dropouts within these distances and the useable distances are now less than half of what was measured above.
What may have changed to cause this change in performance?
I'm really in trouble here if I can't solve this.
This design has also gone through FCC testing without any problems.
Justin
510 843 4500