Hi,
I had made an attempt trying simulate a dual microphone, noise cancellation method, with the Supplies to this circuit is 3.3V and GND.
Below is the snapshot of my circuit, I had also attached my schematic file 7762.PRENOISwSUMAMP_BPF_COM.TSCof my circuit.
What I'm not sure from my circuit is the voltage offset for the op-amps. From past experience, the input offset voltage get amplified at the output and the desired signals get saturated. However, as i simulate this circuit, it's not the case, the output stays at the offset voltage level. So 'im confused here.
Please kindly advise what I should take note of, whenever the op-amp circuit supplies are not dual but V+ connects to 3.3V and V- is to GND.
Awaits reply
Regards
Seng Huat