Other Parts Discussed in Thread: PCM1803A, PCM1802, PCM1803
Hi,
I would like to know besides parametric differences between PCM1802 and PCM1803A, what are the other features that differs between both converters
Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Lee,
I'm not sure I follow your question... Can you clarify?
-d2
Hello Lee,
PCM1802 offers 105dB Dynamic Range with -96dB THD
PCM1803 offers 103dB Dynamic Range with -95dB THD
PCM1802 also includes the analog anti aliasing filter down to 300kHz, which is a significant advantage. (and is costly to add in silicon). The PCM1803 relies on a higher frequency anti aliasing circuit internally (therefor smaller), and the user should add an external filter.
Is that enough to get started?