Other Parts Discussed in Thread: TPA3121D2
I am seeing a strange problem with the Mute signal on a TPA3121D2.
We are using it in an application for a kenwood radio to mute beeps from radio control heads.
It seems like it doesn't mute the output immediately. It's hard to tell when it kicks in, because I only have short 50 ms beeps that are coming through it, but in any case it does not mute the first 50 mS beep after the mute line goes high. I am driving the mute pin from a gpio pin on a PIC microcontroller running at 3.3 volts, so I think I am within VOH of the mute signal. The incoming audio beep comes in 7.6 mS after the mute goes high. Note this application is only mono and uses the LOUT output only.
Is there some delay necessary? What is meant by when muting, the "outputs run at a 50 percent duty cycle"? shouldn't they just be grounded when the mute goes high? Is there a problem since we are only using the LOUT output instead of both ROUT & LOUT?
Should we be using the -SD shutdown input instead of mute?
Thanks,
Vic Elias