Other Parts Discussed in Thread: TAS5558, PCM3070, TAS5548, TAS5631B
Hello,
I actually try to communicate with a TAS5558 PWM IC. There's one more device on the I2C bus which works without problems but the TAS5558 doesn't response. I tried everything, checked the circuit again and again, I even replaced the TAS with no result. Attached you can find my schematic and a few scope screenshots. The valid led sometimes turns on, even then, there is no I2C communication possible.
On pic "signal_r18_c48" you can see the signal between resistor r18 and capacitor c48 (Pin 7/8). Don't know if it's ok and if it has something to do with the problem. You will also find the pics with the clocks so you can see that the clocks are ok. Everything else on the board works fine, except the TAS5558.
My Masterclock runs at 12.288MHz, Wordclock is 96kHz and Bitclock is 6.144Mhz.
Thanks for taking time reading this.
Best regards,
Bernhard Wächter