Other Parts Discussed in Thread: TAS5705, TAS5706, TAS5716, TAS5760M
Hi all,
I2S input power amplifier such as the TAS5705, 06, 16 have sampling frequencies configurable up to 192kHz. However, the maximum audio frequency is not specified.
I would like to know what is the maximum frequency the protocol can handle, given the sampling frequency. In addition, is there any frequency limit given by other artefact such as open or close loop technology?
I know there is at least two other discussions about this topic in this forum. Proposed solutions are PWM input circuits. I would like to understand I2S protocol limitations in ultrasound frequencies.
My application is ultrasound actuator control at 30 to 40 kHz. Output power is 10W. This application includes sinusoid carier generation and level control. Dynamic range is about 20 dB.
Thanks for your support,
Philippe Junod/ R&D engineer