Other Parts Discussed in Thread: TLV320AIC33
Afternoon engineers
I'm working with a TAS1020B evaluation board. The board's really nice, I like it, it does some lovely things.
However my headaches begin with compiling and running the Firmware Development Kit sources, which are the basis for a TAS1020B project. Basically I cannot for the life of me get the code to run past the while loop at line 129 of device.c. So, for me, for some reason, the FDK sources arn't working. I've tried numerous compiler option changes (as well as compiling it straight from the zip file of course) all to no avail and more headaches.
I'm reaching out to someone out there (I know you're there somewhere) for a working base code setup that you've got of the TAS1020B example code, that you've seen working and then built on. Just something that I can then build my stuff on, and eventually work out why my vanilla sources arn't working.
The only thing that definitely works for me on my eval board is the firmware that shipped inside of it, and a firmware image from TI's consultants InDesign, which apparently is the shipped firmware. Which means that i'm struggling to evaluate the the actual chip!
Hope someone can help.
Many more details available on request. Please ask.
Rich