This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PurePath Source code

Other Parts Discussed in Thread: CC8531, PUREPATH-WL-CFG

CC85XXDK-HEADSET said:
"However firmware with USB support is not yet available upon the release of this kit."

CC8531 said:
"Built-in audio protocol
-CD quality uncompressed audio
-Excellent robustness and co-existence through multiple techniques
-Adaptive Frequency Hopping
-Forward Error Correction
-Buffering and Retransmission
-Error Concealment
-Optional high quality audio compression"

PurePath Wireless Configurator PUREPATH-WL-CFG said
"PPWC works on precompiled image files"

PurePathWirelessConfigurator.exe said:
"example projects
preloaded demo
wireless headset
wireless USB headphones"
etc
 
I intend to use the CC85XXDK and IAR 8051 compiler to customize the CC8531.

Where is the source code for the example projects?
Is USB audio source now supported in CC85XXDK-HEADSET?

  • Hi David, 

    Two things:

    1. USB is now supported
    2. The PurePath Wireless Configurator tool is all you need to get you application up and running. This tool will allow you to modify all parameters and specifics for your application and will generate a flash image that can be downloaded to the CC85xx device. We do not open for customization beyond the capabilities already built into the configurator and the EHIF (external host interface). 

    I recommend that you read the User Guide for these devices located here:
    http://www.ti.com/lit/swru250

    This document will go in depth on the capabilities of the device. 

    Best regards,
    Kjetil