This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mc34119 equivalent ic

Dear All

Can you please provide the mc34119 equivalent IC.

Regards

Bala

  • Hi all,

    Can you please respond my problem as soon as possible.

    Regards

    bala

  • Bala,

    Have you tried using the TI product selection tool? Please give this a try..

    For portable audio amp's,, here is the link..

    http://www.ti.com/lsds/ti/audio-ic/dynamic-speaker-product.page

    -Ravi

  • Hi Ravi Singh

    In that it's not having the differential speaker outputs .

    MC34119 IC is Suppoerts following

    Wide Operating Supply Voltage Range (2.0 V to 16 V), Allows
    Telephone
    Line Powered Applications
    • Low Quiescent Supply Current (2.7 mA Typ) for Battery
    Powered Applications
    • Chip Disable Input to Power Down the IC
    • Low Power–Down Quiescent Current (65 µA Typ)
    • Drives a Wide Range of Speaker Loads (8.0 Ω and Up)
    • Output Power Exceeds 250 mW with 32 Ω Speaker
    • Low Total Harmonic Distortion (0.5% Typ)
    • Gain Adjustable from <0 dB to >46 dB for Voice Band
    • Requires Few External Components
    MAXIMUM RATINGS
    Rating Value Unit
    Supply Voltage –1.0 to +18 Vdc
    Maximum Output Current at VO1, VO2 ±250 mA
    Maximum Voltage @ Vin, FC1, FC2, CD
    Applied Output Voltage to VO1, VO2 when disabled
    –1.0, VCC + 1.0
    –1.0, VCC + 1.0
    Vdc
    Junction Temperature –55, +140 °C

    Regards

    Bala