Other Parts Discussed in Thread: CC2590
Hi all,
In my application, CC8531 + CC2590 are used as MASTER(USB Headset) and CC8520 + CC2590 as SLAVE(Remote Headset). When they are pairing closely on sheet metal, wireless communication between them is broken. So, in order to investigate the cause, I measured RSSI value using PurePath Wireless Commander and CC debugger. I conducted RX/TX Test. Here are settings of the test and the result.
↓setting of MASTER side
↓setting of SLAVE side
The result at SLAVE is below.
In the result, the RSSI value measured in the condition that causes communication failure was about -7dBm. According to RF characteristics for CC85xx + CC2590 of CC85xx Datesheet, Saturation (maximum input level) is -12dBm. So, if the RSSI value exceeds -12dBm, is it all right at recognition that a communication failure occur?
Best regards,
Hirokuni Oota