Hello,
When I use the TAS5704, after I release /RESET, the device seems to stay at power down state with VALID pin at low. But if I remove the LRCLK input and power up the TAS5704, then release /RESET, then supply the LRCLK input, the device functions normally with VALID pin goes high. Is this a device bug? In my design, the MCLK input to the TAS5704 is tied high.
BR - Henry