Other Parts Discussed in Thread: PCM9211, MSP430F5325, SRC4190
Hello All,
According to "Table 3. ADC Clock Requirements" on datasheet of PCM9211 , ADC sampling rate can be switched into 44.1Khz, 48Khz, 88.1Khz, 96Khz.
but by setting registers 31h, 33h and 42h , i didn't find any way to set sampling rate on 44.1KHz.
using crystal oscillator of 24.576MHz and MSP430F5325 as control unit.
I need all 3 sampling rate availability with my device.
Any suggestions or help would be welcome and appreciated.
Thanks and regards:-
Sonu Verma