This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC85XXDK Evaluation Module

Other Parts Discussed in Thread: CC8531, CC2590

Using the Purepath Wireless Configurator software I'm successful configuring a 1 master and 1 slave arrangement. I'm unsuccessful configuring 1 master and 3 slave modules. The distributor FAE I deal with for this product was also unsuccessful and I haven't heard a solution from him.

So I'm going direct to TI. Do you have a configuration document that would walk me through the appropriate settings for this arrangement?

Thank you,

Gary.

  • Hi Gary, 

    Just trying the most obvious first. 
    Have you increased the maximum slave count under the 'radio' panel in the PurePath Wireless Configurator for your master configuration?

    Regards,
    Kjetil 

  • Thanks.......arg....that's it. Amazing that the FAE also missed it. We were both focused on the "Slave" section requiring the quantity setting.

    Most appreciated!

    Gary.

  • Hi.

    I'm continuing my evaluation on the CC8531 using the CC85XXDK eval kit.

    At the present time I'm testing for transmission drop outs. I have the slave board 35' from the master and experience a consistent 200mS drop out a few times per hour. (My method is transmitting a constant 1Khz sine wave and scope capturing the drop out duration).

    I've moved the test set to different environments to rule out a strong interfering signal.

    I'm curious and blame the Purepath system because the drop outs are consistently a 200mS duration.

    I also can't believe that TI would have acquired this technology with this issue, and think that it must be a configuration issue.

    Any ideas?

    Gary.

  • Kjetil:

    From my reading of several posts it looks like you can help me with this present issue:

    Hi.

    I'm continuing my evaluation on the CC8531 using the CC85XXDK eval kit.

    At the present time I'm testing for transmission drop outs. I have the slave board 35' from the master and experience a consistent 200mS drop out a few times per hour. (My method is transmitting a constant 1Khz sine wave and scope capturing the drop out duration).

    I've moved the test set to different environments to rule out a strong interfering signal.

    I even experience this problem with the test units outside. Latency presently set to 20mS.

    Any ideas?

    Gary.

  • Hi Gary, 

    Could you please attached your configuration files for me to have a look at?
    Are you using CC85x1 in a USB configuration?

    Regards,
    Kjetil 

  • Hi Kjetil.

    Thanks for your reply. I'm out of the office, I'll send the files to you on Monday.

    Most appreciated,

    Gary.

  • Hi Kjetil:

    I'm using the CC8531 with an analog 2CH input, 2CH output.

    The application is wireless loudspeakers. Maximum configuration is 1 master 4 slaves. I'm using the CC2590 to increase the transmission range.

    I explained my test method above.

    Hopefully the attached file is the one that you requested. It is based on the preloaded examples with slight modifications. This is the file I used to test the 1st level of drop out testing.

    (Don't know if the "Attach file" worked above please advise)

    Thanks,

    Gary.

  • Hi Gary, 

    Answered the original post:
    http://e2e.ti.com/support/low_power_rf/f/382/t/293876.aspx

    Regards,

    Kjetil