Hi,
We have a 5.1 channel application, we use 4 pcs TPA3116D2,
Q1: how to set the master and slave on the 4 parts.
Q2: we now set the bass channel as slave and set other 5 channel as master, the bass channel TPA3116 conected
to one master TPA3116, other 2 TPA3116 is independent. The problem is the temperature of four TPA3116
is higher, about 60C degree even no audio signal input and BLT output through LC filter open.
We think the temperatur is too high. we can not position the root cause.
Can you help on this?