Hi,
I am using TPA3123D2 TI power amplifier for my audio application.
I use BTL mode for amplification.
Please refer the attached xls sheet "Subwoofer ckt" for tpa power amp circuit and speaker connections.
Issue I face is:
I constantly get ~3Hz "DUP DUP" sound at the subwoofer speaker output.
Whatever be the input I feed to TPA3123D2 power amp, I get only 3Hz dup dup output.
Possible problem:
#1 The output LC filter values.
I have found more posts in TI forum where they have discussed about output LC filter causing these kind of issue.
Based on those discussions, I tried removing the LC filter at the TPA output and I found 250KHz PWM output at Lout and Rout of TPA power amp, which I guess is the expected behavior.
I even tried with L=11uH and C=1.3uF at output but still I get 3Hz dup dup output.
Please find the experiments I did for debugging this issue in the sheets of attached xls.
#2. Input pre-amp:
For some reason, I found that bypassing input pre-amp ckt, eliminates the 3Hz dup dup noise.
Setup:
- Circuit used - Please refer the "Subwoofer ckt" sheet of the attached xls.
- TPA3123D2 Supply - 15V bench power supply.
- Pre-amp supply - 15V.
- Speakers - Two 3" 4ohms speakers (derived by parallel'ing four 3" 8ohm speakers). Refer "Subwoofer ckt" sheet of the attached xls.
Kindly help me in debugging the reason for getting 3Hz dup dup output.
Regards,
Karthik