This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48310 RF noise Issue and periodically damaging them

Other Parts Discussed in Thread: LM48310

Hi,

I am using a LM48310 ultra low emi audio amplifier and I am having two issues. They are:

1) Radiated emi in the 2.4 ghz band

2) When output is shorted either to ground or the speaker outputs are shorted appears to damage the device. I thought it had output short circuit protection.

Is there anything I am doing wrong with the filtering on the device or configuration on the input that may be causing these issues? 

Tony

  • Hi, Tony,

    Both are strange; this device is supposed to have good EMC performance, and be fully protected.

    A couple thoughts - how close is your layout to the one shown for the demo board on page 15 of the d/s?

    Pay particular attention to the power, ground, and grounding of the output filter.

    Speaking of the output filter, I would also verify the ferrite beads are optimal. I can't quite tell from your schematic what you're using. You want a relatively high impedance in the MHz range, and be carefuly --> ferrite bead current ratings are based on thermal limits, NOT minimum impedance limits (so your bead may not be acting as a bead at higher currents).

    -d2

  • Hi Don,

    You were correct on the bead not acting as a bead at the higher current limits. We changed the bead to an inductor and optimized the filter and our RF problem went away.  Thanks for your help! It steered us in the correct path to solve this problem. 

    Tony

  • Hi, Tony,

    Glad it worked out! Let us know if you need anything else. I'm going to close this thread.

    -d2