Other Parts Discussed in Thread: PCM1804
The data sheet for the PCM1804 says the typical dynamic range is 112 dB. Is that the dynamic range of the analog input? The data sheet says that the Analog input voltage, full scale is 5 V p-to-p which is about 7 dBu. Can the PCM1804 digitize signals down to -105 dBu? What are the preferred input levels or input range for best performance?
Thanks,
Rich