This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Class D Power Consumption with No Sound using TLV320AIC3262

Other Parts Discussed in Thread: TLV320AIC3262, TLV320AIC3212

I have an ultra-low power consumption application, and I am using the EVM for TLV320AIC3262.  When I power the Class D voltage with a separate DC power supply at 3.3V and start running the Codec for class D output, even with no sound playing (and no speaker connected at all) it starts to draw 18mA from the supply.  The carrier frequency is 250kHz and I can see both the plus and minus outputs switching from Gnd to 3.3V at 250kHz with 50% duty cycle as expected...so is this simply I = C*V*f and we are driving about 20nF of load on the EVM board??  I then took out two 4.7nF caps I saw on the EVM schematic output (C99 and C101) but it was still drawing 14mA.  I don't see any other capacitance the output is driving.  I was planning to make our own PCB with very little capacitance on the class D output to confirm, but we need to get the "no sound" power consumption near 200uA.  Is this just an output capacitance issue??  Thanks for any guidance!! 

Note:  A similar previous post did not fully answer this question.  It was "TLV320AIC3212 Class-D Speaker High Current Consumption Issue in No sound Playing Condition"